Part Number: MSP430I2021
Hi team,
My customer needs every possible option from the compiler to optimize the code size to fit into the FLASH. However they are running into some problems:
There is the option for the silicon version:
In SLAU131R they found:
1. But is the MSP430i2021 an MSP430x device or not?
1a. If not, is there a problem to activate it anyway?
The code size reduction is significant for my customer. A compiler warning is not generated.
2. Is it ok for them to use this option without any drawback?
Also, there is an option for the hardware multiply:
The MSP430i2021 has a 16 Bit hardware multiplier. If they set the optimization to 32 there is no compiler warning and the code is significantly reduced.
Their customer wants this option set to 32 to reduce the code size.
3. Is this a feasible way?
Thanks for the support.
Obinna.