Part Number: MSP430F148
Hello,
This function is called with the ADC 12-bit value of temperature.
The value is a WORD (16-bit) and is converted to a float value
by using the equations according to its value.
For some reason, when I try to set a breakpoint within the
different conditions, only the first one is allowed.
Also the value (1426) is definitely not greater than 3800 -
so why does this row get called?
Is there something about dealing with float values that is specific
with this MSP430?
Thanks for any help and ideas.
Mechi