This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

MSP430FR5994: MSP low-power microcontroller forum

Part Number: MSP430FR5994


Setting the PSEL bit causes the LFXIN and LFXOUT ports to be configured for LFXT operation. If LFXTBYPASS is also set, LFXT is configured for bypass mode of operation. The User's Guide said : LFXIN can accept
an external square-wave clock input signal. 

But My question is: Is it  right to use 32768Hz sine signal (eg. MEMS Ocillator) as the input signal connect to LFXIN? Can FR5994 normally operration?  

Thankyou!

**Attention** This is a public forum