Hello,
According to the datasheet this part is capable of working down to 1V8. I have tried to debug it at this voltage by changing the debugging properties on CCS10:
Project properties/Debug/MSP430Flash Settings
To 1V8, but there is a load error when doing that.
At the default 3V3 it works fine, and all the way down to 2V2 it works, if I put voltages lower than that, it doesn't work.
In order to get the same result I have tried as well, using MSP-FET430UIF, using the VCC_sense option, and supplying an external voltage of 1V8, same error.
Please advice, as the device is in a board with other uP with absolute maximum rating 1V9, so now I can't program it or debug it.
Best regards,