This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

MSP430FR2676: Peripheral Level Code Development

Part Number: MSP430FR2676


Hello All,

I are developing a battery operated device which would have 12 cap-sense Input button, with one I2C based sensor and two UART based sensor interface to it.

For this device we have selected MSP430FR2676 MCU.

I am using CCS 9.2 and MSP ware 3.80.13.03 with Captivate FR2676 developement Kit,

For peripheral development i was referring "MSP430 DriverLib for MSP430FR2xx 4xx Devices" guide.

However i am not able to find any example of related MSP430FR2676 also the examples from driver library doesn't support MSP430FR2676 as i was not ale to find any Board.h file with respect my selected MCU.

I also generated a empty blinky project in CCS but i dint get any driver library adding options.

In MSPware i have also got register level driver codes on the below link 

So my query was,

So do we have to use the register level driver code and then build our own library on top of it ? If yes then is there any relevant document to understand the register level driver code apart from data sheet (If any Please share)?

Thanks and Regards

Utkarsh

**Attention** This is a public forum