Part Number: MSP430FR5994
Hi,team
I'm using MSP430FR5994 Launchpad kit. I'm trying to Initialize clock sources using function "CS_initClockSignal" but when i call function initClock();, i'm getting "#10010 errors encountered during linking ".
I was able to blink LEDs and access switch inputs using another code. For accessing switch, i had to update MSP430FR5994.h file as per given in E2E forum.
The code i used is attached below. Please review.
#include "./MSP430FR5xx_6xx/driverlib.h"
#include <stdio.h>
//#include <driverlib.h>
void initClock(void);
void timer_delay(uint32_t);
int flag1 = 0,flag2 = 0;
int count = 0;
volatile int SW1_state=1,SW2_state=1;
int main(void)
{
volatile uint32_t i;
volatile uint8_t SW1,SW2;
volatile uint16_t SW1_interrupt=1,SW2_interrupt=1,SW1_interrupt_pre,SW2_interrupt_pre;
volatile uint32_t delay = 0;
// Stop watchdog timer
WDT_A_hold(WDT_A_BASE);
initClock();
GPIO_setAsOutputPin(GPIO_PORT_P1, GPIO_PIN0); // Set Red LED output
GPIO_setOutputLowOnPin(GPIO_PORT_P1, GPIO_PIN0); // Red LED off
GPIO_setAsOutputPin(GPIO_PORT_P1, GPIO_PIN1); // Set Green LED output
GPIO_setOutputLowOnPin(GPIO_PORT_P1, GPIO_PIN1); // Green LED off
GPIO_setAsInputPinWithPullUpResistor(GPIO_PORT_P5, GPIO_PIN6); // S1 P5.6: PxDIR, PxOUT and PxREN registers
GPIO_selectInterruptEdge(GPIO_PORT_P5, GPIO_PIN6,GPIO_HIGH_TO_LOW_TRANSITION); // S1 P5.6: PxIES register
GPIO_setAsInputPinWithPullUpResistor(GPIO_PORT_P5, GPIO_PIN5); // S2 P5.5: PxDIR, PxOUT and PxREN registers
GPIO_selectInterruptEdge(GPIO_PORT_P5, GPIO_PIN5,GPIO_HIGH_TO_LOW_TRANSITION); // S2 P5.5: PxIES register
SW1 = GPIO_getInputPinValue(GPIO_PORT_P5,GPIO_PIN6);
SW2 = GPIO_getInputPinValue(GPIO_PORT_P5,GPIO_PIN5);
//SW1_state = SW1 & 0x08;
// Disable the GPIO power-on default high-impedance mode to activate previously configured port settings
PMM_unlockLPM5();
// Set all P5IFG to zero
P5IFG = 0x00;
GPIO_enableInterrupt(GPIO_PORT_P5, GPIO_PIN5);
GPIO_enableInterrupt(GPIO_PORT_P5, GPIO_PIN6);
__bis_SR_register(GIE); // Enable all interrupts
//*
// Enable Switch interrupt
GPIO_clearInterrupt(GPIO_PORT_P5, GPIO_PIN5);
GPIO_clearInterrupt(GPIO_PORT_P5, GPIO_PIN6);
//*/
SW1_interrupt_pre= GPIO_getInterruptStatus(GPIO_PORT_P5, GPIO_PIN6);
SW2_interrupt_pre= GPIO_getInterruptStatus(GPIO_PORT_P5, GPIO_PIN5);
}
/* Initializes Clock System */
void CS_init()
{
// LFXT Setup
// Set PJ.4 and PJ.5 as Primary Module Function Input.
GPIO_setAsPeripheralModuleFunctionInputPin(GPIO_PORT_PJ,GPIO_PIN4 + GPIO_PIN5,GPIO_PRIMARY_MODULE_FUNCTION);
CS_setExternalClockSource(32768, 0); //void CS_setExternalClockSource (LFXTCLK_frequency, HFXTCLK_frequency ) both in Hzl
// Initializes the XT1 crystal oscillator
CS_turnOnLFXT(CS_LFXT_DRIVE_3);
// Set DCO frequency to 16MHz
CS_setDCOFreq(CS_DCORSEL_1, CS_DCOFSEL_4);
// Configure one FRAM wait state as required by the device data sheet for MCLK
// operation beyond 8MHz _before_ configuring the clock system.
FRCTL0 = FRCTLPW | NWAITS_1;
CS_initClockSignal(CS_MCLK,CS_DCOCLK_SELECT,CS_CLOCK_DIVIDER_1);
CS_initClockSignal(CS_SMCLK,CS_DCOCLK_SELECT,CS_CLOCK_DIVIDER_1);
CS_initClockSignal(CS_ACLK,CS_LFXTCLK_SELECT,CS_CLOCK_DIVIDER_1);
}