This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi everyone,
I am looking for E2E forum for MSP430 gang programmer. basically i want support for gang programmer. I am familier with MSP-FETU430IF interface which programs 1 micro. this gang programmer uses hex file and programs 8 micro at a time. In my project i am using incricuit programming feature(SPI-Bi wire). also i want to test my circuit board hardware in which MSP430 is embedded. I know it can be done through DLL commands. but still i need some support about initiating this commands.
so please let me know if somebody worked with this.
Regards,
abhishek
here are couple options for having serial programming for MSP430F2132
1) MSP430F2132 is already supported on many SuperPro programmers:
If you want to have serial gang programmer, SuperPro 5004EGP with 4 x ISP socket will do the job. Also SuperPro 5000 series programmers comes with optional DLL support which allows you to control with a third party tool.
2) SuperPro IS01 is an In-system programmer. Since the requirement is having a gang programmer to program MSP430F2132 on board, having a fast programmer and the largest outcome should be the most important criteria. SuperPro Is01 has ARM9 RISC MCU. It is a stand alone programmer, and getting couple of those units may address the requirements. It also supports many devices including following ones:
MSP430F155
MSP430F156 MSP430F157
MSP430F1610 MSP430F1611
MSP430F1612 MSP430F167
MSP430F168 MSP430F169
MSP430F233 MSP430F235
MSP430F2410 MSP430F2416
MSP430F2417 MSP430F2418
MSP430F2419 MSP430F247
MSP430F2471 MSP430F248
MSP430F2481 MSP430F249
MSP430F2491 MSP430F2616
MSP430F2617 MSP430F2618
MSP430F2619 MSP430FG437
MSP430FG438 MSP430FG439
contact me for more information.
mehmet@xeltek.com.
Do you know how to use MSP GANG programmer with DLL extension. currently, i am programming MSP430 with .hex file. but i want to understand how can i use DLL examples for testing functionality of mcro.
Thanks
**Attention** This is a public forum