Part Number: MSP430FR5969-SP
Other Parts Discussed in Thread: MSP430FR5969, MSPBSL
It is clearly understood that development programming can be achieved using the JTAG interface for program updates and debugging.
Application of the MSP430FR5969 will include using the UART for product communications via half-duplex RS485...
MSP430FR5969 product will be on of several units addressed on the two wire RS-485 bus... all units will communicate with a "master PC" on the bus for telemetry feeds, and accepting operating instructions.
Is it feasible to implement in circuit serial programming such that the MSP430FR5969 can be reprogrammed by the "master" over the same serial interface?