Other Parts Discussed in Thread: LM1117
Hello, I have problems with the msp430fr2355. When I power up the microcontroller, if I disconnect the power source I have to wait few seconds before powering it up again,
If I power the microcontroller immediately, it doesn`t start, If I wait and power it again, it starts.
I don't have hardware reset in my board, I use reset and test pins to program the microcontroller via spy-bi-wire interface, I have 47k pull-up resistor and 1nF capacitor connected to reset.
I use a dc power supply to power the board with 5V and have a linear regulator LM1117 fixed to 3.3V.
The microcontroller has two decoupling capacitors with 10uf and 0.1uF values and an external oscillator of 32.7680KHZ with 2 bypass capacitors of 12pF.
What could be causing this behavior? please, Help.