Part Number: MSP430F149
Hello!
I'm working on program for custom version of MSP430F149 chip and face following problem:
There is peripheral device (read FIFO) mapped to 0x104, 0x106 addresses. GCC compile only first access to it and optimize out all others.
I tried next:
[VERSION_0]
func.h:
uint8_t read_fifo (uint16_t *d_l, uint16_t *d_h);
func.c:
extern volatile uint16_t RFIFO_L;
extern volatile uint16_t RFIFO_H;
uint8_t read_fifo (uint16_t *d_l, uint16_t *d_h) {
*d_l = RFIFO_L;
*d_h = RFIFO_H;
return 0;
}
main.c:
#include "func.h"
int main () {
// Stop the watchdog
WDTCTL = WDTPW + WDTHOLD;
uint16_t d[2];
while (1) {
read_fifo(d, d + 1);
if (d[0] == some_value0 && d[1] == another_value0) {
// some processing
}
else if (d[0] == some_value1 && d[1] == another_value1) {
// another processing processing
}
}
}
/some/path/ti/msp430-gcc/include/msp430f149_symbols.ld:
// added two lines
PROVIDE(RFIFO_L = 0x0104);
PROVIDE(RFIFO_H = 0x0106);
RESULT: there is only first read access to FIFO, which returns zero as expectable, but no any other access (I expected that it will read fifo untill power off).
[VERSION_1]
remove extern volatile declarations from func.c and add to /some/path/ti/msp430-gcc/include/msp430f149.h two lines:
sfr_w(RFIFO_L); sfr_w(RFIFO_H);
RESULT: the same
[VERSION_2]
modify SFR entry length in /some/path/ti/msp430-gcc/include/msp430f149.ld to 0x110 address:
SFR : ORIGIN = 0x0000, LENGTH = 0x0110
RESULT: the same
[VERSION_3]
restore msp430f149_symbols.ld, msp430f149.ld and msp430f149.h, in func.c added defines instead of extern volatile:
#define RFIFO_L (*(volatile uint16_t *)(0x0104)) #define RFIFO_H (*(volatile uint16_t *)(0x0106))
RESULT: the same
What I did wrong and how to tell MSPGCC not optimize access to these volatile variables?
Compilation command:
/some/path/ti/msp430-gcc/bin/msp430-elf-gcc -I/some/path/ti/msp430-gcc/include -mmcu=MSP430F149 -Wall -O0 -msmall -flto -fwrapv -mtiny-printf -I./ -L/some/path/ti/msp430-gcc/include -Wl,-Map,test.map,--gc-sections,--just-symbols,msp430f149_symbols.ld,--oformat=ihex main.c func.c -o MSP430F149.a43
GCC version output:
gcc version 9.2.0 (Mitto Systems Limited - msp430-gcc 9.2.0.50)
Configured with: ../../gcc/configure --target=msp430-elf --enable-languages=c,c++ --disable-nls --enable-initfini-array --build=x86_64-pc-linux-gnu --host=x86_64-pc-linux-gnu --enable-target-optspace --enable-newlib-nano-formatted-io --with-pkgversion='Mitto Systems Limited - msp430-gcc 9.2.0.50'
Thread model: single