This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

MSP430 USB Debugging Interface with Windows7

Hi All,

 I am using MSP430 USB Debugging Interface. I have installed all necessary drivers that come with CD. This JTAG tools works fine on WinXP ( I am able to flash & debug), but I am unable to use it with Windows7, as USB tool is not recognized. Is there any latest driver for Windows7? From where can I download it?

FYI, I am using Image Craft Compiler & NoICE debugger…

 

Thanks & Regards,

Shailendra.

 

 

  • Hi Shailendra,

    I'm not sure the Image Craft supports Windows 7. If you are the customer of Image Craft you can ask for support of Windows 7. If they can not support Win7, you have two possibilities: use only WinXP or switch to alternative development tool which supports Win7.

    I would not recommend to copy Windows7 drivers from other development tools to the Image Craft / NoICE installation, because new drivers may be incompatible with debugger.

    Regards,
    Rosty

**Attention** This is a public forum