Part Number: MSP430F6723
Hi,
in my application I need to generate and read a clock generated by firmware. What is the maximum frequency at which a generic I/O port could opperate. Thank you.
Regards.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: MSP430F6723
Hi,
in my application I need to generate and read a clock generated by firmware. What is the maximum frequency at which a generic I/O port could opperate. Thank you.
Regards.
The maximum pin switching speed is given in data sheet (SLAS731D) Table 5-6; it says (effectively) "as fast as the CPU clock".
As an existence-proof, it is possible to put SMCLK out on PJ.0 [Ref data sheet Table 6-80]. This doesn't give you any choice of frequency, but you can turn it on/off using PJSEL.
If you want to generate a clock using software, you should estimate maybe 3-5 clocks for each transition, and double that to get a full cycle period, so maybe MCLK/9. As a practical matter, you'll eventually have to loop (branch) so you'll need to slow the loop to get a consistent frequency.
Your best bet is a timer, which can give you SMCLK/2 max, but you can adjust it.
Does your mention of "read"ing mean that your MCU needs to interpret this clock as well? Doing that would be quite a bit more expensive.
Fastest port write (assembler instruction) will take 3 CPU cycles, and read (assembler instruction) 2 CPU cycles. Also DMA can be used for coping samples from RAM/flash to port or from port to RAM, and each operation (one DMA copy) will take 2 CPU cycles (CPU is stopped during this proccess).
**Attention** This is a public forum