Part Number: MSP430FR6047
Hi to all!
I'm working with MSP430FR6047 for a flow meter application. My setup require a microcontroller as master and the MSP430FR6047 as slave. They communicate using I2C.
I have a few questions about the configuration parameters:
- My idea is to use (with a little modifications) the header files generated by the Ultrasonic Design Center in my master and with these, update the configuration parameters in the MSP430FR6047. Is this a safe operation or i need to include some other files? Please note that my master isn't a TI microcontroller, so i cant use the TI library. If this operation is hard, there is a better way to update the configuration parameters using the generated files from the Ultrasonic Design Center?
- I have reads that to update the config parameters i need to use the Request Application Configuration Update command (0x96), but is unclear when I must sent this command. I must sent this command before or after sending the configuration parameters?
Best Regards