This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

MSP430F5659: USB PC Host download software

Part Number: MSP430F5659
Other Parts Discussed in Thread: MSP430USBDEVPACK

Hi 

Is the Visual Studio host software still available that is not Python based for USB download? I tried to down load it from the app note(link in red) and it says 'site under maintenance.' It's not in the MSPWARE folder. Thanks,

The USB solution for MSP430™ microcontrollers has been designed to make this process simple and straightforward. The device contains a USB-based on-chip bootstrap loader, and TI provides a Windows source project for downloading firmware that can be quickly customized. This source can be built with Visual C++ 2008 Express, available from Microsoft at no cost. For the USB support software for MSP430 MCUs, see the MSP430 USB Developers Package (MSP430USBDEVPACK). This guide is intended for developers creating a basic USB firmware upgrade system. Those wishing to customize the update process or wanting a deeper look at the underlying bootstrap loader can consult Creating a Custom Flash-Based BSL (SLAA450) and MSP430 Programming Via the Bootstrap Loader

**Attention** This is a public forum