Part Number: MSP430FR5969
Other Parts Discussed in Thread: MSP430WARE
Hi sir,
I have some question for MSP430FR5969.
when I down load the file to MSP430FR5969 it show the msg :
from the specification it show: 64K FRAM, 2 KB SRAM but my output file is 224 KByte.
but it still load as the pic in the file.
my file name is Engr1.out .My question is how big my output file can be?
and the msg show on the "Console" is : MSP430: Flash/FRAM usage is 14068 bytes. RAM usage is 2040 bytes.
Can you explain why the output file 's size is 224K but it stills be loaded into the 64 K FRAM and 2K SRAM of MSP430FR5969?
Thanks.