Hello TI Helpers,
The purpose of the code is to generate PWM on P6.0 pin.
In one of TI code it is written there,
P6DIR |= (BIT0+BIT1+BIT2+BIT3+BIT4+BIT5);
P6SEL0 |= BIT0;
P6SEL0 |= BIT1;
Please help us to understand this code.
Thank you in advance.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello TI Helpers,
The purpose of the code is to generate PWM on P6.0 pin.
In one of TI code it is written there,
P6DIR |= (BIT0+BIT1+BIT2+BIT3+BIT4+BIT5);
P6SEL0 |= BIT0;
P6SEL0 |= BIT1;
Please help us to understand this code.
Thank you in advance.
>P6DIR |= (BIT0+
> P6SEL0 |= BIT0;
This part can be understood from data sheet (SLASEC4D) Table 6-68 as configuring P6.0 as TB3.1, controlled by TB3CCTL1/TB3CCR1.
It's hard to explain the rest without some context. Which TI code is this taken from?
**Attention** This is a public forum