Part Number: MSP430FR6047
USS of MSP430FR6047, can you detect if there is water in the water pipe? Which function should be used?I'm using the demo UltrasonicWaterFR604x_02_40_00_00.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: MSP430FR6047
USS of MSP430FR6047, can you detect if there is water in the water pipe? Which function should be used?I'm using the demo UltrasonicWaterFR604x_02_40_00_00.
Hi,
If there is no water in the pipe, there is no received signals. You might use that to detect whether there is water in pipe.
Best regards,
Cash Hao
Hi,
If you mean that there are bubbles in the tube, you can get some received signals in this case. However, the received signal will be somehow influenced by the bubbles. It is hard to measure the bubbles in water,
Best regards,
Cash Hao
**Attention** This is a public forum