Part Number: MSP430F5172
Other Parts Discussed in Thread: TIDA-00462, , BOOSTXL-SHARP128, MSP430FR5969
Dear TI Team,
We are going to demo an ultrasound application following the example application TIDA-00462 (with MSP430F5172). The boards were manufactured and they seem to work (at least the transmitter side). However, the display meant to work with TIDA-00462 is 430BOOST-SHARP96, which is obsolete. We have checked that BOOSTXL-SHARP128 is pin compatible, but it is not plug and play, and I imagine that a change of drivers for the new display (BOOSTXL-SHARP128) will be needed. I checked the forums and I only found this thread as the closest one: TIDA-00462: TIDA-00462, Example Project don´t start the system. Unfortunately, it seems that there is not any code example for the 128x128 w/ msp430f5172.
In any case, we were wondering if there would be a close reference (even for another platform) that we could use as a start point. Are there drivers already developed in other platforms (MSP low-power microcontrollers) that could be close to TIDA-00462 application?
Looking forward to your answer, and any advice or suggestion is welcome.
Thanks in advance.
Best regards,
Manuel