Part Number: MSP430FR5989
I use CCS to build a project. The running space of the program is between 0x4400 and 0xFFFF. I want to write 1100 bytes of data to the address of 0x10000. I use the function "__data20_write_char" writes 20 bytes at a time. When I finish writing, use the function "__data20_ read_char" When reading char, it is found that there are random check errors in several bytes in the middle area. Here is my code:
int ota_write(unsigned long offset,const unsigned char *pdata,unsigned int size)
{
unsigned int i=0;
for(i=0;i<size;i++)
{
__data20_write_char(offset+0x10000+i,pdata[i]);
}
for(i=0;i<size;i++)
{
if(__data20_read_char(offset+0x10000+i)!=pdata[i])
{
DBG_LOG("CHK ERR"); //Several random byte check failures
return -1;
}
}
return 0;
}
static unsigned char test_buf[20]={0};
void test_fram()
{
int i=0,j=0;;
for(i=0;i<55;i++)
{
for(j=0;j<sizeof(test_buf);j++)
{
test_buf[j]=j;
check+j;
}
if(ota_write(i*sizeof(test_buf),test_buf,sizeof(test_buf))!=0)
{return ;}
}
}
Please help me analyze what the problem is.