This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Miniaturisation of ez430rf2500

We now have a basic ez430rf2500 system working and are looking at new applications that require miniturisation of the remote system.
The current board has a footprint of 2cm x 3cm
We are interested in this device with two further footprints 1cm x 1cm and 2mm x 2mm
Can you suggest how we should go about realising this?

 

  • Hi John,
    did you already check Amber Wirless or Anaren

    http://www.amber-wireless.de/index.php?article_id=1&clang=1
    http://www.anaren.com/

     

  • Dear Thomas

    thanks for quick reply.

    I am in contact with Anaren but was unaware of Amber Wireless.

    I'll contact them.

    regards

    John

  •  Dear Thomas

    We are in the process of connecting the a-d of our ez430rf2500 to external peripheral devices.

    We are thinking of connecting a set of Molex pins to P1 - P18, so that we can easily connect/disconnect the ez430rf2500 to different peripherals without damaging it.  

    Unfortunately the USB housing will get in the way of our Molex pins making it very difficult to program the device without removing the housing.

    What we really need is a female to male 6-way extension cable between the USB Degugger board and the ez430rf2500 board.

    Could you tell me what is the make of the 6-way connector between the USB Debugger and the ez430rf2500 board so I can order an 6-way extension? 

    regards

    John Cosmas

**Attention** This is a public forum