Hello Sir,
One of customers is doing water meter. The run rate is 100Ku/Y.
According to our 2LC water meter program guidelines, after installation, the equipment is turned on and the metal disk of the water meter needs to run for a period of time for calibration then it can start to do normal calibration. But the customer's water meter may not be calibrated immediately after installation and the water meter can not process measurements. This will cause user losing their information.
1. Based on upon issue, can the customer save parameters after calibration sot that these parameters can recover after installation?
2. Based on question 1), if those parameters can recover, what's parameters need to be saved and how to do recovery?
Up to now, the customer is trying to save ESIDAC1R0-ESIDAC1R7 values after calibration but the code will not go to Set_DAC function for calibration. This will cause the interrupt of ESI not working normally and measurements are not correct issues...
Hope to get your helps soon,.
Best regards,
wenting