Part Number: MSP430FR5969-SP
Hi experts!
My customer has the following questions. Can someone confirm what is possible, or the potential limitations?
Need a quick clarification: On the space grade MSP430FR5969-SP microcontroller, the block diagram shows 3 comm modules, where two support UART, SPI, and IrDA (eUSCI_A0 and A1), and the third supports SPI and I2C (eUSCI_B0). Just need to know if I can assign 1 module for UART, and the other two for SPI or SPI/I2C? Is there any clocking or data rate limitations when assigning the first two modules to different interface formats?
The block diagram shows eUSCI_A0 and eUSCI_A1 overlapped as if there are ties between the two, and I need to operate them as completely independent as possible.
Thanks for your help!
Best regards,
Jim B