Part Number: MSP430F5529
I am operating the MSP as a slave device, and i use DMA to accomplish the data transfers. I have a ISR thats called when the SS is disabled. like the examples the first thing i check is if the spi is busy.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: MSP430F5529
I am operating the MSP as a slave device, and i use DMA to accomplish the data transfers. I have a ISR thats called when the SS is disabled. like the examples the first thing i check is if the spi is busy.
I've never tried this but my guess is that the DMA has pre-loaded TXBUF (->shift register) with a byte which won't be sent until the next transaction, so it's just sitting there. This would occur if the DMA length is greater than the number of bytes the master actually asked for.
Generally, this pre-loading is a good thing, since that first byte is immediately available when the master starts the transaction. But it does mean everyone has to count the bytes just right.
**Attention** This is a public forum