Part Number: MSP430F417
Hello to everyone. I want to check the variables of the pin to which the step motor is connected from the live watch window in iar. The project's debugger setting is in simulation. Can you tell me where I went wrong?
here is my code:
#include "io430.h"
#include "in430.h"
int voltage ;
void main( void )
{
void Delay(int j);
// Stop watchdog timer to prevent time out reset
WDTCTL = WDTPW + WDTHOLD;
P6DIR|=0XFF;
P6SEL &= ~BIT4;
P6OUT |=BIT4;
Delay(50);
while(1){
P6OUT = (P6IN & voltage);
}
}
void Delay(int j)
{
int i;
for(j=0;j<100;j++)
for(i=0;i<0xFFFF;i++);
}