This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

MSP430G2955: MSP430G2955 low power

Part Number: MSP430G2955

I have a question of MSP430G2955 power consumer. MSP430G2955+ 3.6864MHz oscillator , our power consumption test is 1.8mA but your spec is less than 200uA, when i change the clock into DCO, the consumption is 450uA

#include "include_all.h"
void main( void )
{
// Stop watchdog timer to prevent time out reset
_DINT();
WDTCTL = WDTPW + WDTHOLD;

BCSCTL1 |= XTS; // ACLK = LFXT1 = HF XTAL
BCSCTL3 |= LFXT1S_2; // 3 - 16MHz crystal or resonator

do
{
IFG1 &= ~OFIFG; // Clear OSCFault flag
for (unsigned char i = 0xFF; i > 0; i--); // Time for flag to set
}
while (IFG1 & OFIFG); // OSCFault flag still set?

BCSCTL2 |= SELM_2+DIVM_2+SELS+DIVS_3; // MCLK = XT2/4=0.9216MHz ;SMCLK=XT2/8=460.8kHz

while(1);

}
This is my complete code

**Attention** This is a public forum