Part Number: MSP430F67651A
Hi,
I got a question from my customer using MSP430F67651A.
He wonders whether it is possible to input high frequency clock (~24MHz) to XT1.
Register configuration :
UCSCTL1:0021h(DISMOD=1b(Modulation disabled))
UCSCTL4:0000h(SELA=SELS=SELM=000b(XT1CLK))
UCSCTL6:C13Dh(XT1DRIVE=00b、XTS=1b、XT1BYPASS=1b、XT1OFF=1b)
In datasheet, only LF mode is supported, so HF is not usable, but he wants to double check.
Thanks and regards,
Koichiro Tashiro