Hello,
I have an application that periodically powers on and powers off the MSP430 and the MSP430 needs to read the Pins and do some processing work and read/save values in the FRAM, the power on time is 200µs, which means MSP430 should do all the work within 200µs. I measured the startup time(from power on to first line of code setting a Pin high) on LP-MSP430FR2476, which was above 750µs, my question is , is it at all possible to reduce the startup time to, say 50µs? Or is it possible in other MSP430 types? Thanks.
regards,
Bing