This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LP-MSP430FR2476: ADC result of sample code is not correct

Guru 14810 points

Part Number: LP-MSP430FR2476

Hi,

I am using the sample program as-is to check if the ADC can operate from 0 to 3.3V.

https://dev.ti.com/tirex/explore/node?node=AAd0vOkxyuq9x4RH2X0xZg__IOGqZri__LATEST

However, the ADC pins are always receiving about 0.7V, and I cannot measure voltages below 0.7V.

Is it a specification that 0.7V is applied?

Evaluation board :LP-MSP430FR2476

Thanks,

Koki

**Attention** This is a public forum