This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

MSP430FR2100: using both BSL UART and SPI

Genius 5840 points

Part Number: MSP430FR2100

Hello,

I would like to use BSL UART and SPI.

BSL UART is used for programming firmware at mass production.

So in PW16 package, 11 pin and 12 pin are used.

SPI is used for application to communicate other MCU.

So I am considering following pin assign.

1pin : SCLK

15pin :SIMO

16pin :SOMI

Is this use case no problem?

Regards,

U-SK

**Attention** This is a public forum