Part Number: MSP430FR2533
Hello,
My customer is considering to use MSP430FR2533 with liquid tolerant touch.
But they are plan to develop the board with 6mm air gap and 1.5mm acrylic overlay.
And they want to pass IEC61000-4-3 test.
We recommended bridge material between acrylic and electrode, but they don't want to use it in terms of cost.
Do you think above can be achieved?
Or, is bridge materials mandatory?
The number of buttons is 10, and the size of biggest button is 4.5 cm2.
Regards,
U-SK