Part Number: EVM430-FR6047
HI,
I'm using the Ultrasonic Sensing Design Center with a DN25 pipe, and the Water Meter Constant reaches max value before flow actually being right.
I also use this calibration program connected to a DN15 pipe, and although this constant is almost max out, flow rate is correct in [L/H].
Is there a parameter or a way to lower Water Meter Constant if it's maxing out?
Thanks.