Part Number: EVM430-FR6043
Other Parts Discussed in Thread: MSP430F5528, , UNIFLASH, MSP430FR6043
How to program the interfacing IC's(M430F5528) in EVM Board.
If its possible please the code for the above IC.
Regards,
AK
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: EVM430-FR6043
Other Parts Discussed in Thread: MSP430F5528, , UNIFLASH, MSP430FR6043
How to program the interfacing IC's(M430F5528) in EVM Board.
If its possible please the code for the above IC.
Regards,
AK
Hi AK,
The MSP430F5528 is programmed with a utility called "EZ FET". You can learn how to program this device with this utility in the MSP Debugger's User's Guide:
https://www.ti.com/lit/ug/slau647o/slau647o.pdf
BR,
Leo
I have a 2 development boards of EVM430-FR6043, In which one boards uart and debug IC must be loaded.
Is that possible to load program to the above IC using other EVM Board?
Regards,
AK
Hi AK,
Are you trying to program the FR6043 on one board with the FET from another EVM?
BR,
Leo
Im trying to program F5528 (UART &programming IC) in EVM Board.
To Be more specific please refer the image

Regards,
AK
Hi Akash,
You should be able to do this. For the USB/UART bridge, you'll need the same image that is used in the captivate programmer:
https://www.ti.com/tool/CAPTIVATE-PGMR
BR,
Leo
Hi Akash,
You should be able to use the EzFET from one EVM(signals on J100) to program the EzFET on another EVM. If you want to also program the USB to I2C/UART bridge F5528 you will need to connect to the J200 header.
This thread provides the firmware:
BR,
Leo
Hi Leo,
I tried with the above example, HIDBRIDGE is getting programmed and the comm port is not getting detected after programmed.
The ezfet throws an error stating device has been secured while programming.
Is there anyway to clear this issue
Regards,
AK

Checked with other ezfet board.
Loaded EZFET_Rev1_2_BSL_1_2_noHs file in uniflash, the below error is received.
Regards,
AK
Hi Akash,
The FET shouldn't be locked. Please accept my friend request to discuss further.
BR,
Leo
When loaded EZFET code in uniflash it fails to load, but HID brdige is getting programmed
Regards,
AK
Hi Akash,
Can you confirm whether you are trying to program a working EVM or a target board?
BR,
Leo
Hi Leo,
We made a HIDbridge and Ezfet Part (Interface Part) of the EVM Board. and Im trying to program that interfacing part.
With this Interfacing Board we will program and communicate with the MSP430FR6043 and receive Ultrasonic Readings.
Regards,
AK
Hi Akash,
Can you confirm that when you try to program the F5528 part on the EVM from TI, that this doesn't give an error?
BR,
Leo
Hi Leo,
When tried to program the HID firmware it doesnt five any error,
but when tried to flash the ezfet and BSL firmware it gives error. ( I couldnt load the firmware in uniflash. The MCU is detected and could flash sample program of F5528 in both the MCU.
Regards,
AK
Hi Akash,
I forgot to mention, there is already a small interface/programming board that you can use for this purpose available from TI:
https://www.ti.com/tool/CAPTIVATE-PGMR
Is this useful?
BR,
Leo
Hi Leo,
Yes you have mentioned it earlier, but we need to program the device we made.
Just need a clarification about the bianries sahred from TI, as the binary for EZFET can't be loaded in uniflash, but HIDbridge binary is flashed in both the MCU. So the MCU is working fine but EZFET Binary has some errors in it.
Regards,
AK
Hi Akash,
Please download the Debugger Stack found here and try the ezFET image included with this download:
BR,
Leo
**Attention** This is a public forum