Part Number: MSP430I2041
(Sorry. I made a mistake in the "Part Number" when I posted this article, and used I2021. The correct part number is I2041.)
Hi experts,
My customer is planning to use a 16MHz external oscillator with MSP430I2041. I am referring to the original question, but let me check just to be sure about the case of MSP430I2041.
Q1: When using a 16MHz external oscillator, the SD24 is supplied with a 1MHz clock. But the accuracy at 1MHz is not described in the datasheet, so they have to make sure they meet the requirements themselves. Is this correct?
Q2: When using a 16MHz external oscillator, is there any other possible effect on the SD24?
For example, effects on serial communication such as UART baud rate, etc. I understand that there is not expected to be any long term impact on the device.
Referring to the contents of the datasheet and user's guide, we plan to tell customers that the recommended basic premise is to use 16.834MHz for the external oscillator.
Best regards,
O.H