This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

MSP430FR2675: About capacitive sensor malfunction

Part Number: MSP430FR2675

Hi experts,

Currently my customer has created a prototype board using MSP430FR2675, but occasionally malfunctions occur with the input of the electrostatic sensor.

The phenomenon: they are using the electrostatic sensor as a touch switch and there are 4 electrostatic switches. Touching the switches changes the mode of the user product. But occasionally, after changing the mode, all the electrodes respond even though the switch is not touched. (4 electrode switches reacting at the same time)

Detailed situation: This time, on the MSP430 side, only the function of the electrostatic sensor and the GPIO are working.(and UART for DesignCenter)

  • When power is turned on, the device is in Mode0 and all three GPIOs are in Low state.
  • By pressing SW1, it changes to Mode1 and changes the combination of the three GPIOs at the same time. (H,H,L)
  • By pressing SW2, it changes to Mode2 and changes the combination of 3 GPIOs at the same time. (H,H,H)

Normally, after changing to Mode2, each electrode switch will respond normally. However, sometimes, after changing to Mode2, all the electrode switches respond. (They confirmed in DesignCenter that all electrodes have equal capacitance change.) It takes about 5 seconds for all 4 to be pressed.(There is no finger near the control SW.) Pressing SW1 turns off the power and returns to Mode0. The moment the product enters Mode2 on the product side, the amount of current changes, and it appears to be occurring at that time.



Question: After pressing a capacitive touch switch like this one, is there a pattern where the capacitance is affected at the same time? Or have you seen similar cases in the past?

There is a possibility that this is a customer's board (hardware) factor, so we are continuing to verify this, but any insight or information from TI would be appreciated.

Best regards,
O.H

  • Hello O.H,

    There are several possible causes: HW (PCB), sensor, sensor tuning values, software, and the MSP430.

    Question: After pressing a capacitive touch switch like this one, is there a pattern where the capacitance is affected at the same time? Or have you seen similar cases in the past?

    Regarding the questions, if the sensors are tuned properly with correct thresholds, there is no reason why all of the buttons would be affected. Each button should respond only when that button is touched.

    Can the customer share their schematic and pcb gerber files?  If proprietary, we can setup an E2E "friendship" and share privately.

    Also, can the customer provide their CAPT_UserConfig.c and .h files?

  • Hello Dennis Lehman,

    Thank you for your support.

    I will see if the customer can share the schematic, PCB Gerber file, electrode specifications, CAPT_UserConfig.c and .h files. If we can't share them here, we will set up a "Friendship" and contact you individually.

    Best regards,
    O.H

  • Hi O.H

    It's been a few days since I have heard from you so I’m assuming your customer was able to resolve their problem.
    If this isn’t the case, please click the "This did NOT resolve my issue" button and reply to this thread with more information.
    If this thread locks, please click the "Ask a related question" button and in the new thread describe the current status of your issue and any additional details you may have to assist us in helping to solve your issues.

  • Hi Dennis Lehman,

    Sorry for the late reply.

    Please let me share the data after friend request for customer's unique usage.

    Best regards,
    O.H

  • Hi O.H,

    I accepted your friend request.

  • Hi O.H,

    I have responded in a private message.

  • I am closing this thread because it is being support privately.

**Attention** This is a public forum