Part Number: MSP430F67791A
Hello TI Team,
I am using this EMDC library to read current and voltage. Is it possible to get data of current less than 5ms and voltage in 20ms.
Thanks,
Rahul
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: MSP430F67791A
Hello TI Team,
I am using this EMDC library to read current and voltage. Is it possible to get data of current less than 5ms and voltage in 20ms.
Thanks,
Rahul
Hi Rahul,
You can use the approach described in the linked FAQ thread to get data out faster than every 1 second (default). For your case, I would highly recommend waiting until a full AC cycle has been measured for both VRMS and IRMS. These values are calculated as the root-mean-square across one or more complete AC cycles. Thus, I would recommend the minimum update period (how often the results are updated and sent out) to be no less than 20 ms assuming your nominal AC input frequency is 50 Hz. Keep in mind that depending on the number of phases, ADC sampling frequency, etc. you may need to increase the UART baud rate to ensure that the data gets sent out fast enough.
**Attention** This is a public forum