Other Parts Discussed in Thread: MSP430F5529
We can able to configure the clock of Msp430f5529 for 16MHZ. We required to run the clock at the maximum speed supported by the controller 25MHZ but we unable to do that.We are using Code Composer Studio v4.2.3
For 12Mhz we used below code – we can able to get Lock
WDTCTL = WDTPW+WDTHOLD; // Stop WDT
UCSCTL3 |= SELREF_2; // Set DCO FLL reference = REFO
UCSCTL4 |= SELA_2; // Set ACLK = REFO
__bis_SR_register(SCG0); // Disable the FLL control loop
UCSCTL0 = 0x0000; // Set lowest possible DCOx, MODx
UCSCTL1 = DCORSEL_5; // Select DCO range 24MHz operation
UCSCTL2 = FLLD_1 + 374; // Set DCO Multiplier for 12MHz
// (N + 1) * FLLRef = Fdco
// (374 + 1) * 32768 = 12MHz
// Set FLL Div = fDCOCLK/2
__bic_SR_register(SCG0); // Enable the FLL control loop
// Worst-case settling time for the DCO when the DCO range bits have been
// changed is n x 32 x 32 x f_MCLK / f_FLL_reference. See UCS chapter in 5xx
// UG for optimization.
// 32 x 32 x 12 MHz / 32,768 Hz = 375000 = MCLK cycles for DCO to settle
__delay_cycles(375000);//
// Loop until XT1,XT2 & DCO fault flag is cleared
do
{
UCSCTL7 &= ~(XT2OFFG + XT1LFOFFG + DCOFFG);
// Clear XT2,XT1,DCO fault flags
SFRIFG1 &= ~OFIFG; // Clear fault flags
}while (SFRIFG1&OFIFG); // Test oscillator fault flag
We tried for 24 Mhz with the below code – we unable to get lock
//******************************************************************************
// MSP430F552x Demo - Software Toggle P1.1 with 25MHz DCO
//
// Description: Toggle P1.1 by xor'ing P1.1 inside of a software loop.
// ACLK is rought out on pin P1.0, SMCLK is brought out on P2.2, and MCLK
// is brought out on pin P7.7.
// ACLK = REFO = 32kHz, MCLK = SMCLK = 25MHz
//
// MSP430F5529
// -----------------
// /|\| |
// | | P1.0|-->ACLK
// --|RST P7.7|-->MCLK
// | P2.2|-->SMCLK
// | |
// | P1.1|-->Port Pin toggle
//
// Bhargavi Nisarga
// Texas Instruments Inc.
// April 2009
// Built with CCSv4 and IAR Embedded Workbench Version: 4.21
//******************************************************************************
#include <msp430f5529.h>
void SetVcoreUp (unsigned int level);
void main(void)
{
volatile unsigned int i;
WDTCTL = WDTPW+WDTHOLD; // Stop WDT
UCSCTL3 |= SELREF_2; // Set DCO FLL reference = REFO
UCSCTL4 |= SELA_2; // Set ACLK = REFO
__bis_SR_register(SCG0); // Disable the FLL control loop
UCSCTL0 = 0x0000; // Set lowest possible DCOx, MODx
UCSCTL1 = DCORSEL_5; // Select DCO range 24MHz operation
UCSCTL2 = FLLD_1 + 749; // Set DCO Multiplier for 24MHz
// (N + 1) * FLLRef = Fdco
// (749 + 1) * 32768 = 24MHz
// Set FLL Div = fDCOCLK/2
__bic_SR_register(SCG0); // Enable the FLL control loop
// Worst-case settling time for the DCO when the DCO range bits have been
// changed is n x 32 x 32 x f_MCLK / f_FLL_reference. See UCS chapter in 5xx
// UG for optimization.
// 32 x 32 x 24 MHz / 32,768 Hz = 750000 = MCLK cycles for DCO to settle
__delay_cycles(750000);
// Loop until XT1,XT2 & DCO fault flag is cleared
do
{
UCSCTL7 &= ~(XT2OFFG + XT1LFOFFG + DCOFFG);
// Clear XT2,XT1,DCO fault flags
SFRIFG1 &= ~OFIFG; // Clear fault flags
}while (SFRIFG1&OFIFG); // Test oscillator fault flag
/* Enable interrupts */
__bis_SR_register(GIE);
while(1)
{
// P1OUT ^= BIT1; // Toggle P1.0
__delay_cycles((unsigned int)600000); // Delay
}
}
We tried for 25 Mhz with the below TI sample code – we unable to get lock
//******************************************************************************
// MSP430F552x Demo - Software Toggle P1.1 with 25MHz DCO
//
// Description: Toggle P1.1 by xor'ing P1.1 inside of a software loop.
// ACLK is rought out on pin P1.0, SMCLK is brought out on P2.2, and MCLK
// is brought out on pin P7.7.
// ACLK = REFO = 32kHz, MCLK = SMCLK = 25MHz
//
// MSP430F5529
// -----------------
// /|\| |
// | | P1.0|-->ACLK
// --|RST P7.7|-->MCLK
// | P2.2|-->SMCLK
// | |
// | P1.1|-->Port Pin toggle
//
// Bhargavi Nisarga
// Texas Instruments Inc.
// April 2009
// Built with CCSv4 and IAR Embedded Workbench Version: 4.21
//******************************************************************************
#include <msp430f5529.h>
void SetVcoreUp (unsigned int level);
void main(void)
{
volatile unsigned int i;
WDTCTL = WDTPW+WDTHOLD; // Stop WDT
P1DIR |= BIT1; // P1.1 output
P1DIR |= BIT0; // ACLK set out to pins
P1SEL |= BIT0;
P2DIR |= BIT2; // SMCLK set out to pins
P2SEL |= BIT2;
P7DIR |= BIT7; // MCLK set out to pins
P7SEL |= BIT7;
// Increase Vcore setting to level3 to support fsystem=25MHz
// NOTE: Change core voltage one level at a time..
SetVcoreUp (0x01);
SetVcoreUp (0x02);
SetVcoreUp (0x03);
UCSCTL3 = SELREF_2; // Set DCO FLL reference = REFO
UCSCTL4 |= SELA_2; // Set ACLK = REFO
__bis_SR_register(SCG0); // Disable the FLL control loop
UCSCTL0 = 0x0000; // Set lowest possible DCOx, MODx
UCSCTL1 = DCORSEL_7; // Select DCO range 50MHz operation
UCSCTL2 = FLLD_1 + 762; // Set DCO Multiplier for 25MHz
// (N + 1) * FLLRef = Fdco
// (762 + 1) * 32768 = 25MHz
// Set FLL Div = fDCOCLK/2
__bic_SR_register(SCG0); // Enable the FLL control loop
// Worst-case settling time for the DCO when the DCO range bits have been
// changed is n x 32 x 32 x f_MCLK / f_FLL_reference. See UCS chapter in 5xx
// UG for optimization.
// 32 x 32 x 25 MHz / 32,768 Hz ~ 780k MCLK cycles for DCO to settle
__delay_cycles(782000);
// Loop until XT1,XT2 & DCO stabilizes - In this case only DCO has to stabilize
do
{
UCSCTL7 &= ~(XT2OFFG + XT1LFOFFG + DCOFFG);
// Clear XT2,XT1,DCO fault flags
SFRIFG1 &= ~OFIFG; // Clear fault flags
}while (SFRIFG1&OFIFG); // Test oscillator fault flag
while(1)
{
P1OUT ^= BIT1; // Toggle P1.0
__delay_cycles(600000); // Delay
}
}
void SetVcoreUp (unsigned int level)
{
// Open PMM registers for write
PMMCTL0_H = PMMPW_H;
// Set SVS/SVM high side new level
SVSMHCTL = SVSHE + SVSHRVL0 * level + SVMHE + SVSMHRRL0 * level;
// Set SVM low side to new level
SVSMLCTL = SVSLE + SVMLE + SVSMLRRL0 * level;
// Wait till SVM is settled
while ((PMMIFG & SVSMLDLYIFG) == 0);
// Clear already set flags
PMMIFG &= ~(SVMLVLRIFG + SVMLIFG);
// Set VCore to new level
PMMCTL0_L = PMMCOREV0 * level;
// Wait till new level reached
if ((PMMIFG & SVMLIFG))
while ((PMMIFG & SVMLVLRIFG) == 0);
// Set SVS/SVM low side to new level
SVSMLCTL = SVSLE + SVSLRVL0 * level + SVMLE + SVSMLRRL0 * level;
// Lock PMM registers for write access
PMMCTL0_H = 0x00;
}
We need to run the clock at 25Mhz , the maximum speed supported by msp430f5529.
Where we went wrong
Thanks in advance
Regards,
Vinoth.S,