Other Parts Discussed in Thread: MSP430F5438
Hi,
I'm wondering where the interrupt vectors are specified. From the example code for the F5438 device I can find the following vector:
// Timer A0 interrupt service routine
#pragma vector=TIMER1_A0_VECTOR
__interrupt void TIMER1_A0_ISR(void)
{
P1OUT ^= 0x01; // Toggle P1.0
}
but also:
// Timer_A3 Interrupt Vector (TAIV) handler
#pragma vector=TIMER1_A1_VECTOR
__interrupt void TIMER1_A1_ISR(void)
{
switch(__even_in_range(TA1IV,14))
{
case 0: break; // No interrupt
case 2: break; // CCR1 not used
case 4: break; // CCR2 not used
case 6: break; // reserved
case 8: break; // reserved
case 10: break; // reserved
case 12: break; // reserved
case 14: P1OUT ^= 0x01; // overflow
break;
default: break;
}
}
If I'm going to use another interrupt, how do I know what range it has and what interrupt happens at what place in the vector?
/Adde