Other Parts Discussed in Thread: TPS2041B
I would like to power this launchpad from an external 5V USB battery pack. However, 5V and 3.3V is not detected at the isolation jumpers. Only when a USB from a computer is used will the 5V and 3.3V rails can be detected at the jumpers. The voltage seems to stop at U401 for 5V and U403 for 3.3V. These 2 ICs are nowhere to be found on the schematic. My guess is that they are load switches for the two rails. My question: Is there a correct way to power from an external USB like a battery pack or a wall wart or is there an easy to bypass the load switches by depopulating a component or 2 without needing to hack the board with wires and such.
Thanks,
Jordan