Hello,
I’m using the msp430f5438A, with CCs 5.3.
And I want to use with the I2C module ( my first time) in order to read data from I2c simulator (AARDVARK I2c simulator)
I get the following wave diagram:
i use the following code:
****************************************
int main(void)
{
Uint16 rslt = 0;
Uint16 tmpDelay = 10;// init value.
__bic_SR_register(GIE); // disable interrupt.
PortCnfg();
ClockCnfg();// 16mhz
TimerA1Cnfg();//timer interrupt of 10Hz.and blink the led
I2cCnfg ();
__bis_SR_register(GIE); // enable interrupts
while (1)
{
rslt = I2cRd ( 3);// read 3 data
while ( tmpDelay--)// delay between conversion.
{
__delay_cycles(30000);
}
tmpDelay = 1;
}
}
void I2cCnfg (void)
{
UCB1CTL1 |= UCSWRST; // Enable SW reset
//The USCI module is configured as an I2C slave by selecting
//the I2C mode with UCMODEx = 11 and
//UCSYNC = 1 and clearing the UCMST bit
// also, UCSSELx bits is Modify only when UCSWRST
UCB1CTL0 = UCMST + UCMODE_3 + UCSYNC; // I2C, Master, synchronous mode
UCB1CTL1 = UCSSEL__SMCLK + UCSWRST;// Use SMCLK, keep SW reset
UCB1CTL1 &= UCTR;// config as read (DEFAULT).
UCB1BR0 = 160; // fSCL = SMCLK/160 = ~100kHz
UCB1BR1 = 0;
UCB1I2CSA = 0x48; // Slave Address is( 16 bits) 048h
UCB1CTL1 &= ~UCSWRST; // Clear SW reset, resume operation
}
Uint16 I2cRd ( Uint16 numRd)
{
Uint16 NumOfRd = numRd;
UCB1CTL1 &= ~UCTR;// config as read.
// this section is for reading.
while (UCB1CTL1 & UCTXSTP); // Ensure stop condition got sent
// ensure to close any open transaction
// before you start new one
UCB1CTL1 |= UCTXSTT; // I2C start condition/transaction.
// __no_operation();
while(UCB1CTL1 & UCTXSTT); // Start condition sent?
__no_operation(); // For debugger
while (NumOfRd--){// number of reading, without repeated start
while (!(UCB1IFG & UCRXIFG));//UCRXIFG is automatically reset when UCxRXBUF is read
I2cRdData [I2cRdIndx] = UCB1RXBUF;
I2cRdData [I2cRdIndx] |= ((UCB1IFG & UCNACKIFG) == 0)? 0: 0xF000;// recording nack/ack.
//UCNACKIFG is automatically cleared when a START condition is received.
UCB1IFG &=~ UCNACKIFG;// clear manually.
I2cRdIndx++;
I2cRdIndx%=I2C_RX_BUF_SIZE;
}
UCB1CTL1 |= UCTXSTP;// I2C stop transction
return TEST_OK;
}
***************************************
I want to emphasize:
1. all the data read correctly from the simulator ( 0xFF 0x01 0x00)
2. in the above code , i record the data and the accompanying nack/ack . no nack is record. the nack recognize
only by scope. without observing the data by the scope i wouldn't recognize the problem.
is anyone can explain the Nack appearance ?
thanks.