Other Parts Discussed in Thread: MSP-FET
Hi, I am able to download free license of CCS V6. Example codes compiled properly. While downloading code, it displays following message ,
MSP430: Error initializing emulator: A firmware update is required for the MSP430 Debug Interface (MSP-FET430UIF / MSP-FET / eZ-FET). Click the "Update" button to update the firmware and launch your debug session (this may require several update steps). DO NOT UNPLUG THE INTERFACE DURING THE UPDATE.
MSP430: Error: MSP-FET / eZ-FET legacy module update failed.
Tried to update , but it fails.
Ez-FET of 5969 launchpad is detected as “MSP Application UART1”.
But it is not shown in CCS to connect to target.
Kindly suggest.
Regards
Atul Bhakay