This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

10mA constant current source independent of load (10 ohm to 5k ohm)

Dear all,

I want to design a constant current source of 10 mA which will not vary on load connected.

Is there any IC available for it?

My load will vary from 10 ohm to 5k ohm. 

I have tried using discrete components (Howland current source but i unable to achieve 10mA current. Howland source gives me 5.2mA constant current at 12V voltage)

Please suggest me good circuit or IC 

I have attached the circuit which i simulated. if I change the value of resistances below 2.3k then current is not getting constant through 5K load

**Attention** This is a public forum