Part Number: MSP430I2021
Hi all,
first of all, I am new to the IEC60730 topic and I'm aware that the software libraries developed by TI do not support the MSP430i2xx family.
Never the less I was trying to make adaptions to the downloadable source code of the library (MSP430 IEC60730 software package version 1.20.00.03).
I modified the linker files to the processors's needs but I am running into a compiler error:
"../lnk_msp430i2021.cmd", line 98: error #10099-D: program will not fit into available memory. run placement with alignment fails for section ".safe_ram" size 0x0 error #10010: errors encountered during linking; "IEC60730_emptyProject.out" not built
This error got me thinking whether or not it is possible to implement the IEC60730 standards on the MSP430i2xx family at all? Or does TI not recommend this processor family for the IEC60730 standard?
Thanks in advance for your inputs.
Janine