This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

MSP430G2553: MSP430G2553 Clock Speed

Part Number: MSP430G2553

Hi all:

I am having trouble figuring out this problem. Maybe someone here can give me some ideas. I am using the TI MSP430 Launchpad. 

I have fixed  the MSP430G2553 clock speed at 8 MHz in the code, and according to the datasheet, the clock speed should increase with increasing voltage. However, when I measure it using DCO calibration technique, I get a decreasing clock speed with increasing voltage. The variation is not too much; it varies between 7.92 to 8.16MHz. But shouldn't it be fixed at 8MHz, or maybe increase? I see nothing in the datasheet that explains this anomaly. 

Any ideas?

**Attention** This is a public forum