Other Parts Discussed in Thread: ADS1298
Tool/software: TI-RTOS
Hi,
I have been developing a product using the TI MSP432P401R, TI ADS1298 analog-to-digital converter, and TI-RTOS with TI Drivers (SPI in my case). I'm using the SPI Driver and TI-RTOS from the last version of SimpleLink MSP432 SDK. In few words, my application configures the ADS1298 and put in CONTINUOUS conversion mode. The ADS1298 has a pin that generates an interrupt when a conversion is done. I have opened the SPI Driver in blocking mode. In my first application, the interrupt pin callback post a semaphore and unblock a task that read the data from ADS calling SPI_trasfer() function, but the interrupt frequency (related with sample rate from ASD1298) is faster than system tick (1 ms), and the task will always run and not allowing others to run. So, I change my program, opening SPI driver in callback mode. Then, the interrupt pin callback calls SPI_transfer() in the Hwi context and SPI callback store the data in a buffer. When the buffer is completely filled, the SPI callback posts a semaphore and the task is unblocked and process the chunk of data.
I have read the TI-RTOS 2.20 user guide and is not clear to me if SPI_transfer can be called from callback context (Hwi). I have searched for a clarification in the e2e forum but no e2e thread answers my question. The closest e2e thread that I have read https://e2e.ti.com/support/embedded/tirtos/f/355/t/513722 In some e2e posts, the people say that is possible call SPI_transfer() from callback. In another say that is not possible. I'm really confused.
There is a better way to do what I have been trying?
Can someone help me?
Thanks in advance!