This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

MSP430FR2532: Setting baudrate 115200 for MSP430

Part Number: MSP430FR2532

Hi,

My system (MSP430FR2532) working perfectly for baudrate 9600. But when I change baudrate to 115200, it does not work; I check on the scope and found that the duration for 1 bit is 10us (instead of 8.6us of the correct bit for baudrate 115200). Please help to check if I am missing anything? Thank you.

#define MCLK                    (8000000L)  /* MCLK Frequency in Hz */
#define CONFIG_CI_PHYDL_UART_BAUDRATE        (115200)

#if (MCLK==8000000)
#   if (CONFIG_CI_PHYDL_UART_BAUDRATE == 9600)
#       define UCOS16_VAL   1
#       define UCBRx_VAL    52
#       define UCBRSx_VAL   0x49
#       define UCBRFx_VAL   1
#   elif (CONFIG_CI_PHYDL_UART_BAUDRATE == 57600)
#       define UCOS16_VAL   1
#       define UCBRx_VAL    8
#       define UCBRSx_VAL   0xF7
#       define UCBRFx_VAL   10
#   elif (CONFIG_CI_PHYDL_UART_BAUDRATE == 115200)
#       define UCOS16_VAL   1
#       define UCBRx_VAL    4
#       define UCBRSx_VAL   0x55
#       define UCBRFx_VAL   5
#   else
#       error "Baudrate is not supported"
#   endif
#else
#error "Frequency is not supported"
#endif

/******************************************************************************
 *
 * @brief   Initializes UART
 *
 * @return  none
 *****************************************************************************/
//inline static void clock_init(void)

void TI_MSPBoot_CI_PHYDL_Init(t_CI_Callback * CI_Callback)
{
    UCA0CTLW0 = UCSWRST | UCSSEL_2;          // USCI held in reset and use SMCLK

    //P1SEL0 &= ~(BIT4 | BIT5);                 // Enable P4[2:3] for USCI_A0 UART mode
    //P1SEL1 |= (BIT4 | BIT5);                //
    P1SEL0 |= BIT4 | BIT5;

    UCA0BR0 = (UCBRx_VAL & 0xFF);           // Set Low baudrate byte
    UCA0BR1 = (UCBRx_VAL >> 8);             // Set high baudrate byte
    UCA0MCTLW = UCOS16_VAL |                 // Set modulation values
              (UCBRSx_VAL << 1) | 
              (UCBRFx_VAL << 4) ; 
    /*UCA0BR0 = 4;                                        //UCBR = INT(N/16) = 4
    UCA0BR1 = 0;
    UCA0MCTLW |= 0x5500 + UCBRF_5 + UCOS16;*/
    
    UCA0CTLW0 &= ~UCSWRST;                   // Clear SW reset, resume operation
  
    // Initialize all callbacks
    CI_Callback_ptr = CI_Callback;
    // Init state machine
    CI_State_Machine = USCI_STATE_IDLE;
}

/******************************************************************************
 *
 * @brief   Initializes the MSP430 Clock
 *
 * @return  none
 *****************************************************************************/
//inline static void clock_init(void)

static void clock_init(void)
{
    // Configure one FRAM waitstate as required by the device datasheet for MCLK
    // operation beyond 8MHz _before_ configuring the clock system.
    /**************************************************/
    WDTCTL = WDTPW | WDTHOLD;
    //FRCTL0 = FRCTLPW | NWAITS_1;

    __bis_SR_register(SCG0);                           // disable FLL
    CSCTL3 |= SELREF__REFOCLK;                         // Set REFO as FLL reference source
    CSCTL0 = 0;                                        // clear DCO and MOD registers
    CSCTL1 &= ~(DCORSEL_7);                            // Clear DCO frequency select bits first
    CSCTL1 |= DCORSEL_3;                               // Set DCO = 8MHz
    CSCTL2 = FLLD_0 + 242;                             // DCOCLKDIV = 8MHz
    __delay_cycles(3);  
    __bic_SR_register(SCG0);                           // enable FLL
    while(CSCTL7 & (FLLUNLOCK0 | FLLUNLOCK1));         // FLL locked
    
    CSCTL4 = SELMS__DCOCLKDIV | SELA__REFOCLK;        // set default REFO(~32768Hz) as ACLK source, ACLK = 32768Hz
                                                       // default DCOCLKDIV as MCLK and SMCLK source
    PM5CTL0 &= ~LOCKLPM5;                     // Disable the GPIO power-on default high-impedance mode
                                              // to activate previously configured port settings
    
    __delay_cycles(1000);
    
}

regards,

Quang

  • Hi Quang,

    It looks like in your TI_MSPBoot_CI_PHYDL_Init function, you should be shifting UCBRSx_VAL by 8 instead of 1 to set the proper bits in UCA0MCTLW.

    So

        UCA0MCTLW = UCOS16_VAL |                 // Set modulation values
    
                  (UCBRSx_VAL << 1) |
    
                  (UCBRFx_VAL << 4) ;

    should become

        UCA0MCTLW = UCOS16_VAL |                 // Set modulation values
    
                  (UCBRSx_VAL << 8) |
    
                  (UCBRFx_VAL << 4) ;

    When I tested your code with this update, the code was able to communicate at a baud of 115200. It seems like 9600 baud is slow enough that having the UCA0MCTLW values from your initial code did not affect the clock rate enough to cause errors.

    Regards,

    Ryan

  • Hi Ryan,

    Thank you so much for the expeditious answer. The system work perfectly with baudrate 115200 now.

    cheers,
    Quang

**Attention** This is a public forum