Part Number: MSP432E401Y
Other Parts Discussed in Thread: MSP-EXP432E401Y
Tool/software: TI-RTOS
Dear TI-Experts,
when I activate PD7's pull up or pull down with GPIOPadConfigSet I cannot see any change of the pad's voltage (load >10Meg Ohm).
Is this pin somehow locked? I couldn't find any remark in SLASEN5 or SLAU723. Only the fact that it can be configured as NMI attracted my attention. I actually use it as ADC input. Enabling pull-up or pull-down is intended to check the board to controller connection. The mechanism works with all other pins but PD7.
Any idea?