This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Tool/software: Code Composer Studio
Hi,
importing in CCS 8.2 an Energia sketch which uses a Adafruits GFX library, there are two compiliation errors in msp430_MSP_EXP430FR2433LP_Adafruit_GFX. In Energia everything is working as intended. Just wondering if anyone had the same error and knows how to get this running in CCS (since I'd like to use the nice EnergyTrace monitoring).
Thanks in advance.
Regards,
Robert
fontconvert/subdir_rules.mk:7: recipe for target 'fontconvert/fontconvert.o' failed
22:22: fatal error: ft2build.h: No such file or directory
Hi,
the Adafruit GFX core library can be found here. The display-specific library PL_microEPD for little Epaper screens can be found here.
This is the sketch, working fine in Energia:
#include "Adafruit_GFX.h" #include "PL_microEPD.h" #include <SPI.h> #define EPD_RST 17 #define EPD_BUSY 8 #define EPD_CS 13 PL_microEPD display(EPD_CS, EPD_RST, EPD_BUSY); void setup() { SPI.begin(); SPI.beginTransaction(SPISettings(6000000, MSBFIRST, SPI_MODE0)); display.begin(); display.println("Hello World!"); display.update(); } void loop() { }
Thanks for your support,
Robert
**Attention** This is a public forum