Part Number: TM4C1292NCPDT
Hello,
Section 17.3.4 of the data sheet states that the SSInFss signal can be programmed to assert low at the start of each frame for enhanced modes of operation. This raises a fewquestions:
Is 'advanced SSI mode' per section 17.3.3 and 'enhanced modes' per section 13.3.4?
If so, then how does it differ from legacy mode with an 8 bit frame? In particular, the FSSHLDFRM bit of register SSICR1 does not appear to require that the MODE field be set to a mode other than legacy for SSInFss to be pulsed once per frame? In general, how does legacy 8 bit mode differ from advanced SSI mode with 8 bit packet size?
Looking at firgure 17-5, in datasheet section 17.3.7.3, timing for Freescale SPI format, the bit clock SSInClk stays low for more than a half clock cycle between frames. But, no specification seems to give its exact timing, nor the relationship to SSinFss. The text below the figure describes the timing, but ambiguities remain. What specification for SSInClk timing and SSInFss timing for Freescale SPI format with SPO=0 nad SPH=0?
Thank you.