Other Parts Discussed in Thread: UNIFLASH,
Hi.
Is there any equivalent this command from Keil in CCS?
In Keil, I can use
const unsigned short CHECKSUM __attribute__((section(".ARM.__at_0xF0000"))) = 0x0F88;
and then I can open binary file and change the value at the address 0xF0000 to anything I want.
but I can't find anything in CCS 10.1.
I want to reserve 4 bytes of memory at special memory in .bin file so I can do the CRC and save the CRC value at that memory in Binary file. Later I can read it back and display it on an LCD screen.
I have tried with
#define DEFAULT __attribute__((at(0x400))) = 0x10
but when I open bin file with HxD and look at address 0x400. It is not correct value so my define is not correct.
Anyone can help ?