Other Parts Discussed in Thread: UNIFLASH
I am trying to use CCS Uniflash with an XDS100v2 debugger to unlock a device that I have locked a section of memory to be read only. The unlock and finish unlock appear to work, but the device is not programmable after I power cycle it. My original program also continues to run so the memory is not being erased as it should with this operation. I am attaching a screenshot of the entire sequence:
What could cause this operation to fail? We are using daisy chained JTAG with two processors, but the one I am trying this operation on is the first in the chain. Could this be the problem? Is there a known problem with the Uniflash 3.4 release?
Thanks for the help,
Cam
<NOTE> Edited the title to show version 3.4 is being used, not 3.1.